Technical FAQs

Ask a Question

The new EZM 2000A main has cu bus. Can you use meter stacks that have al bus or must they be cu also?

Can use stacks that have al or cu bus. Just make sure the cross bus of the stacks is rated 1200A not 800A as the main must be center located.


CTA-ID : 2023649
Was this helpful?
What can we do to improve the information ?