Technical FAQs

Ask a Question

The C60L has 440vac ratings. What are the 480vac ratings (Icu) for the C60L?

Unfortunately we never made any tests at more than 440V for C60L. And the only test at 480Y/277V we made was on C60N for your UL range (breaking capacity 5kA). Then as C60L is better than C60N for breaking capacity, then we can say it will accept the same 5kA without any problem but I can`t give you more without any proof.

CTA-ID : 2023853
Was this helpful?
What can we do to improve the information ?