Technical FAQs

Ask a Question

Can I put a 1200A EZM31200CB main circuit breaker into an inside corner 90 degrees and install a branch section around the corner, or would extensions be needed?

Use an extension EZM3EXT with a corner device for clearance purposes.

CTA-ID : 2023657
Was this helpful?
What can we do to improve the information ?