Technical FAQs

Ask a Question

Do you have to use the load neutral on a HOM230EPD breaker?

No. If the load itself does not have a neutral, the neutral terminal does not have to be connected. This would be for a 240vac load on a 120/240 system.

CTA-ID : 2023645
Was this helpful?
What can we do to improve the information ?