Technical FAQs

Ask a Question

What are the repair parts for the H363AWA, series F6 (may be shown as F06)?

The repair parts for the H363AWA, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly - 4056775150 (requires one. Arc Suppressor not included)
-Load Base Assembly - 4056614550 (requires one)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one)
-Arc Suppressor Mounting Screw - 4020514501 (requires one)
-Lug Assembly - 4025601450 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056787350 (NOTE: also recommend replacing Switch Mechanism Gasket and Handle Gasket)
-Switch Mechanism Gasket - 4056786001
-Mechanism Washer - 2360200008
-Handle Assembly - 4056663550 (also recommend replacing Handle Gasket)
-Handle Gasket - 4056603101
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Rod/Linkage Assembly - 4056787150
-Receptacle - WRDK1034 (mounting screws included)
-Ground Lug - 4025101851 (3 total required)
-Ground Lug Mounting Screw - 4020514801 (longer screw) and 4020513503 (shorter screw) - 1 each
-Fuse Pullers - FPK0610 (1 required)


CTA-ID : 2023563
Was this helpful?
What can we do to improve the information ?