Technical FAQs

Ask a Question

Is it possible to field convert the Class 9422 Type TDF60 disconnect from 60 amp 250 volt to 60 amp 600 volt fuse clips?

Yes, order Class 9422 Type TD63 fuse clip conversion kit which includes line side fuse clips and a complete fuse base assembly.

CTA-ID : 2023839
Was this helpful?
What can we do to improve the information ?