Technical FAQs

Ask a Question

Can two partitions be installed in the 10`` or 18`` wide wall duct, if the run contains a tee?

Yes. You would use the tunnel kit for 3 compartment tees - catalog number RWT10PTE or RWT18PTE.


CTA-ID : 2023638
Was this helpful?
What can we do to improve the information ?