Technical FAQs

Ask a Question

If I use a 400A busplug on a vertical riser application, does it still take up two openings on the bus as the 400A units do in a horizontal application?

Yes. Busplugs of this type take up two openings on the bus whether in a vertical riser or horizontal configuration.


CTA-ID : 2023637
Was this helpful?
What can we do to improve the information ?