Technical FAQs

Ask a Question

What is the handle padlock attachment for an FH, FHL breaker?

Issue:
What is the handle padlock attachment for an FH, FHL breaker?

Product Line:
Circuit Breakers
Legacy

Environment:
Electrical Distribution Equipment

Cause:
Application the needs a field installed padlock attachment.

Resolution:
The number is a HPAFK, which locks the break in the ON or OFF position.


CTA-ID : 2023486
Was this helpful?
What can we do to improve the information ?