Technical FAQs

Ask a Question

What are the catalog numbers for Base Unit for the XVE Indicator Banks?

XVEC21 is Nema and UL Type 12 and IP42 rated. XVEC21P is IP54 rated.


CTA-ID : 2023830
Was this helpful?
What can we do to improve the information ?