Technical FAQs

Ask a Question

Are the I line panelboards rated for DC voltages?

Issue:
Are the I line panelboards rated for DC voltages?

Product Line:
I Line Panelboards

Environment:
Application

Cause:
Specification requirement

Resolution:
I Line panels can operate up to 250V DC. and up to 250A for branch breakers. There are no DC rated Powerpact breakers above 250A that are DC rated


CTA-ID : 2023819
Was this helpful?
What can we do to improve the information ?