Technical FAQs

Ask a Question

Customer asks if a LAL3640036M is CE marked.

The Mag-Gard breakers are not CE marked with the exception of the GJL type circuit breakers.


CTA-ID : 2023471
Was this helpful?
What can we do to improve the information ?