Technical FAQs

Ask a Question

Can a XX518A3PAM12 detect a rod of 2.5 mm diameter at approximately 7 inches of range? Will it detect 4 / second?

The published specification is detection of a 2.0 mm rod at 8 inches. The sensor will detect the rod inquired about. Published response time is 15 milliseconds on / off. Four rods per second equal 250 milliseconds / rod. The sensor will detect four / second with no problem.

CTA-ID : 2023792
Was this helpful?
What can we do to improve the information ?