Technical FAQs

Ask a Question

What is the size of the standard HVL viewing window and how high is it above the floor? What material is used for the window?

The window is 5-1/2`` high x 21-1/2`` wide. The centerline of the window is 67-1/2`` from the floor for indoor and 71-1/2`` for outdoor. It is made of a Lexan type plastic.


CTA-ID : 2023788
Was this helpful?
What can we do to improve the information ?