Technical FAQs

Ask a Question

When does the LUA8E20 control circuit contacts change state?

When used in conjunction with the Standard or Advanced control module the contacts change state on a short circuit, overload, and when the rotary operator is in the off position. When used with the Multi-function control module the contacts change state on short circuit or if rotary operator is in the off position but does not change state on overload.


CTA-ID : 2023491
Was this helpful?
What can we do to improve the information ?