Technical FAQs

Ask a Question

Are gold flashed contacts available for a XB4 or XB5 push buttons and selector switches ?

Yes , use a ZBE1016 normally open block or ZBE1026 normally closed block . These are rated 24vac and .1a max and additional blocks cannot be stacked behind these .

CTA-ID : 2023410
Was this helpful?
What can we do to improve the information ?