Technical FAQs

Ask a Question

What is the dv/dt on the output of the ATV58HC10N4XZU?

The peak voltages for the HHP unit is 2600V/us (Volts per microsecond).
The information in this resolution should be used with discretion as it is not standard published information.


CTA-ID : 2023616
Was this helpful?
What can we do to improve the information ?