Technical FAQs

Ask a Question

What is the catalog number for an optional neutral lug to add to a Combination Service Entrance Device neutral assembly?

LK100AN accepts 1-#6 to 2/0 and can be used with Meter Main Types RC, SC, QC and All-In-One Types SC, SU< QC and RC.

CTA-ID : 2023615
Was this helpful?
What can we do to improve the information ?