Technical FAQs

Ask a Question

What is the acceptable conductor sizes for the LUB12, LUB32, LU2B12 or LU2B32 starters?

Power Terminals - One or Two #16 to #8 AWG conductors.
Control Terminals - One or Two #18 to #14 AWG conductors.


CTA-ID : 2023057
Was this helpful?
What can we do to improve the information ?