Technical FAQs

Ask a Question

What is the Total amp capacity of the 24V supply on ATV31?

The maximum available current is 100mA. (It is min. 19 V, max. 30 V for logic inputs)


CTA-ID : 2023130
Was this helpful?
What can we do to improve the information ?