Technical FAQs

Ask a Question

Are NEMA style overload relays available with auto reset?

The only offering in the Class 9065 are the bimetallic versions listed on page 14-98 and Motor Logic Plus listed on page 14-97 of Digest 173.

CTA-ID : 2023749
Was this helpful?
What can we do to improve the information ?