Technical FAQs

Ask a Question

Does the Graphic Display (keypad) come with the Altivar 71 drive or is it ordered separetly?

The units that are stocked in Mechanicsburg will include the Graphic Display.
The smaller units (20HP or less) can be ordered without the keypad by adding a Z to the end of the part number but, there are no plans to stock this version.

CTA-ID : 2024195
Was this helpful?
What can we do to improve the information ?