Technical FAQs

Ask a Question

Can a HOM115 be used on two separate circuits?

Yes it can be done. But check the local code to see if it is allowed.


CTA-ID : 2023422
Was this helpful?
What can we do to improve the information ?