Technical FAQs

Ask a Question

What is the resistance to vibration for the ATV31?

Issue:
What is the resistance to vibration for the ATV31?

Product Line:
ATV31

Environment:
All

Cause:
Specifications

Resolution:
Conforming to IEC/EN 60068-2-6: 1.5 mm peak to peak from 3 to 13 hz, 1 gn from 13 to 150 hz.

 
Was this helpful?
What can we do to improve the information ?