Technical FAQs

Ask a Question

What is the part number for the interior trim and cover for a QO440M225RB?

Issue:
Need replacement interior trim and/or cover for a QO440M225RB

Product Line: 
QO load centers

Environment:
Load Centers:

Cause:
Repair parts

Resolution:
The part numbers were 40548-022-05 for the cover and 40505-704-01 for the deadfront. Both of these parts are now complete obsolete.
Was this helpful?
What can we do to improve the information ?