Technical FAQs

Ask a Question

Q13100 Circuit Breaker Replacement

Issue:
What is the replacement for the Q13100 circuit breaker in an obsolete NQO panelboard?

Product Line:
Obsolete NQO panelboards that were sold and supported in the USA.

Environment:
Replacement/maintenance

Cause:
Is there a replacement for a Q13100 in the obsolete NQO panelboard?

Resolution:
The suggested replacement is a QO3100 for a 3 phase NQO panelboard or 3 phase load center . The SK5669 mounting assembly is used to branch mount both the old Q1 and newer QO breakers in the NQO and is not required for replacement purposes. 


 
Was this helpful?
What can we do to improve the information ?