Technical FAQs

Ask a Question

What is the interrupting rating of a NX361200 breaker?

Issue:
What is the interrupting rating of a NX361200 breaker?

Product Line:
Legacy Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Interrupt Ratings below:

125K @ 240V
100K @ 480V
65K @ 600V

For addition information please see catalog 0612CT9201.

http://static.schneider-electric.us/docs/Circuit%20Protection/Molded%20Case%20Circuit%20Breakers/OBS%20PE/0602CT9201R201.pdf


CTA-ID : 2023750
Was this helpful?
What can we do to improve the information ?