Technical FAQs

Ask a Question

What size panel screw is a p/n 80025-067-01? Also what size driver is needed for the head?<br /><br />

10-32 x 7/16. This screw head takes a #2 square driver.


CTA-ID : 2023596
Was this helpful?
What can we do to improve the information ?