Technical FAQs

Ask a Question

What components are supplied with the Class 9421 Type LR1 circuit breaker operating mechanism?

Includes (1) Class 9421LH6 handle operator, (1) 9421LL1 operating mechanism and (1) 9421LS8 shaft.


CTA-ID : 2023580
Was this helpful?
What can we do to improve the information ?