Technical FAQs

Ask a Question

What is the catalog number for the device that takes two pole spaces to mount in a QO load center and is similar to a circuit breaker except that it has lugs only to give a feed thru option?

There are several devices, according to ampere rating:
QO60SL is a two pole, 60A rated plug on sub feed lug kit
QO2125SL is two pole, 125A rated sub feed lug kit.
NOTE: There is also the following which requires 4 pole spaces to mount:
QO2225SL is a two pole, 225A rated sub feed lug kit, and it may be used only in single phase load centers

CTA-ID : 2023747
Was this helpful?
What can we do to improve the information ?