Technical FAQs

Ask a Question

Does the DT363 Double Throw Safety Switch include a neutral?

Issue:
Product Features

Product Line:
Double Throw Safety Switch

Cause:
Clarification of standard features

Resolution:
No, it does not. If a neutral is needed, order SN0310 separately for field installation. 



CTA-ID : 2023742
Was this helpful?
What can we do to improve the information ?