Technical FAQs

Ask a Question

Is the handle operator on the VCFN12GE and VCFN20GE enclosed Mini-Vario switch padlockable?

Yes, will accept (1) padlock with 0.32 inch or 8 mm shank or (3) padlocks with 0.24 inch or 6 mm shank.


CTA-ID : 2023741
Was this helpful?
What can we do to improve the information ?