Technical FAQs

Ask a Question

What is the lever arm operating force for the 9007C limit switch?

Type A, B, T10 and T5 heads are 4 lbs-inch
Type N head is 25 oz-inch
Type C head is 3 lbs-inch

CTA-ID : 2023737
Was this helpful?
What can we do to improve the information ?