Technical FAQs

Ask a Question

What is the Terminal Lug Data for the H365AWK, Series E4 (E04) and Series E5 (E05) Heavy Duty safety switch?

Issue: 
Wire size for 400amp NEMA 12 heavy duty safety switch

Product Line:   
Heavy Duty Safety Switches

Environment:   
Switch Line and Load Terminal Sizes

Cause:  
Installation of appropriate wire sizes for the Line and Load of the H365AWK heavy duty safety switch.

Resolution:  
The terminal lug data for the H365AWK Series E4 (may be shown as E04), and E5 (may be shown as E05) will accept up to (1) #1/0 - 600 kcmil or (2) #1/0 – 300 kcmil Al/Cu conductors per phase. 

NOTE: THERE ARE NO OPTIONAL LUGS AVAILABLE.
 



CTA-ID : 2023521
Was this helpful?
What can we do to improve the information ?