Technical FAQs

Ask a Question

Is the TIKFD required to install an EDB EGB, or EJB circuit breaker in an NF panelboard?

No, although listed on the Digest page with the branch circuit breakers, this accessory is not required when applying the EDB, EGB or EJB branch breakers in an NF panelboard.  This kit is used when making a hard bus termination on the load side rather than using wire.


CTA-ID : 2023369
Was this helpful?
What can we do to improve the information ?