Technical FAQs

Ask a Question

Can the 9001 Type B control stations (ex; 9001BW240) be used on DC voltages?

Yes. 5 Amps - Continuous Carrimg Amperes.
120V DC - 1.1A Make and Break Amperes
240V DC - 0.55A Make and Break Amperes
600V DC - 0.2A Make and Break Amperes

See Digest 173 page 17-101 for AC voltages ratings.


CTA-ID : 2023281
Was this helpful?
What can we do to improve the information ?