Technical FAQs

Ask a Question

What is the temperature range for the GS1 disconnects?

The temperature range is -20 to +40 degrees C. (-4 to +104 degrees F)


CTA-ID : 2035510
Was this helpful?
What can we do to improve the information ?