Technical FAQs

Ask a Question

What is the mechanical and electrical life for the 9050JCK timing relays?

These products have 10 million Mechanical operations (No load, 18,000 operations/hr maximum) and 100,000 Electrical operations (1,800 operations/hr maximum). These are at an operating temperature of -18 to 104 degrees F, or -28 to 40 degrees C.


CTA-ID : 2035497
Was this helpful?
What can we do to improve the information ?