Technical FAQs

Ask a Question

What is required to assemble two LC1D80 int a reversing pair?

For AC controlled devices:
Mechanical Interlock with Electrical Interlocks - LA9D4002 or Mechanical Interlock without Electrical Interlocks - LA9D50978.
Reversing Power Conductors, line and load side - LA9D8069.

For DC controlled devices:
Mechanical Interlock with Electrical Interlocks - LA9D8002 or Mechanical Interlock without Electrical Interlocks - LA9D80978.
Reversing Power Conductors, line and load side - LA9D8069.
For the AC application, use cat. no. LA9D4002 and for the DC application, use cat. no. LA9D8002.


CTA-ID : 2022920
Was this helpful?
What can we do to improve the information ?