Technical FAQs

Ask a Question

Are optional lugs available for a DJM circuit breaker used in an EZMK311400 branch device?

Optional lugs are available in a kit containing three lugs to change all three poles on one end of the circuit breaker. Optional field installed lug kit, catalog number 32510, provides lugs for (2) #2/0 AWG - 350 kcmil copper or (2) #2/0 AWG - 500 kcmil aluminum conductors. The standard lug kit, catalog number 32508, provides lugs for (1) #2 AWG - 600 kcmil copper or (1) #2 AWG - 500 kcmil aluminum conductor.
NOTE: The optional lug referenced is for the DJM circuit breaker only. It is not an optional lug for the branch neutral bar.

CTA-ID : 2023354
Was this helpful?
What can we do to improve the information ?