Technical FAQs

Ask a Question

What is the terminal data for the MG/MJ frame breaker (300A to 800A)?

Standard lugs are for three 3/0 to 500 kcmil cables per phase aluminum or copper. Lug kit AL800M23K, 3 lugs per kit.


CTA-ID : 2023681
Was this helpful?
What can we do to improve the information ?