Technical FAQs

Ask a Question

What information is available on the standard HVL viewing window?

The standard window is Lexan plastic and is 21.5`` across x 5.75`` high. For indoor switches the centerline of the window is 67`` up from the floor.

CTA-ID : 2023703
Was this helpful?
What can we do to improve the information ?