Technical FAQs

Ask a Question

How does the ATV58 drive calculate power when Analog output is set to Output Power?

The drive estimates the kW based on motor voltage and amps and the phase angle.


CTA-ID : 2023530
Was this helpful?
What can we do to improve the information ?