Technical FAQs

Ask a Question

What is the maximum number of contacts that can be used on a 8501XUDO relay.<br />

The maximum number of normally contacts is 12.


CTA-ID : 2023117
Was this helpful?
What can we do to improve the information ?