Technical FAQs

Ask a Question

What are the repair parts for the HU362WC, series F6 (may be shown as F06)?

The repair parts for the HU362WC, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly -40566-091-50 (includes all poles. Arc suppressor assembly not included)
-Line Base Mounting Screw - 40205-151-01(3 required)
-Arc Suppressor Assembly - 40566-355-50 (requires one per switch)
-Arc Suppressor Mounting Screw - 40205-145-01
-Lockplate - 40566-721-01
-Lockplate Mounting Screw - 22999-405-62 (2 required)
-Handle Assembly - 40566-635-50
-Switch Mechanism - 40567-873-50
-Rod/Linkage Assembly - 40567-870-50
-Lug Kit - AL0306F (one kit includes all line and load lugs)
-Receptacle - 25410-023-11
-Receptacle Mounting Screws - 45102-801-01 (required 4)


CTA-ID : 2023493
Was this helpful?
What can we do to improve the information ?