Technical FAQs

Ask a Question

What is the difference between the QOU120 and QOU120VH ?

The QOU is rated at 10K AIR, the QOUVH is rated at 22K AIR at 120vac.


CTA-ID : 2023879
Was this helpful?
What can we do to improve the information ?