Technical FAQs

Ask a Question

Do the SquareD/Schneider Electric Sealed Resin Epoxy Encapsulated Transformers contain copper windings?

Issue:
Specifications often call for copper windings on Sealed Resin Epoxy Encapsulated Transformers

Product Line:
LV Transformers

Environment:
Applies to Sealed Resin Epoxy Encapsulated Transformers by SquareD/Schneider Electric

Cause:
The most common transformer winding materials are aluminum and copper

Resolution:


Yes. All Sealed Resin Epoxy Encapsulated Transformers are wound with copper wire.


CTA-ID : 2023878

Was this helpful?
What can we do to improve the information ?