Technical FAQs

Ask a Question

Which side of MP85200 is the three-gang side and which is the two-gang side?

Two meter sockets are on the left and three are on the right. See CAD drawing 2529 (Top Left Position Omitted on 5-gang Unit).

CTA-ID : 2023875
Was this helpful?
What can we do to improve the information ?