Technical FAQs

Ask a Question

Can the SCS parameter be utilized in the Powersuite software to save current configuration to EEPROM and then recall the settings using the FCS rEC1?

No. These parameters and operation can not be performed with Powersuite.
Under configurations it is possible to go back to Factory settings. However it is not possible to recall a saved set of customer initiated parameters that were stored on the EEPROM.
To perform this action, recall would have to be done by the keypad on the drive.
Powersuite can be used to store additional files on a computer.

Reviewed 7/2011

CTA-ID : 2023386
Was this helpful?
What can we do to improve the information ?