Technical FAQs

Ask a Question

What is the replacement fuse part# for the S33595 Full Function Test Kit?

We do not sell the replacement fuses. Recommendations are:
For 120 Vac Applications: 2 A, 250 Vac, Fast-blow. (Bussman Part No. AGC-2)
For 230 Vac Applications: 1 A, 250 Vac, Fast-blow. (Bussman Part No. AGC-1)


CTA-ID : 2035485
Was this helpful?
What can we do to improve the information ?